AXIS#.PL.INTOUTMAX

Description

AXIS#.PL.INTOUTMAX limits the output of the position loop integrator by setting the output saturation.

When used in concert with AXIS#.PL.INTINMAX, this variable allows you to make the position loop integrator effective near the target position. Far from the target position, however, the integrator is not dominant in the loop dynamics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Velocity Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.INTOUTMAX

500ch

09h

Signed32

Position

-

Read/Write

No

AXIS2.PL.INTOUTMAX

510ch

09h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5906

1

5906 (0x1712)

AXIS1.PL.INTOUTMAX

Signed32

Read/Write

Yes

71442

2

5906 (0x1712)

AXIS2.PL.INTOUTMAX

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.INTOUTMAX

5906

Float

Read/Write

Velocity